Choose a Category

A Complete Guide to Gears

What is a Gear?

The use of gears dates all the way back to the 27th century B.C.E. A Chinese emperor is credited with designing a chariot that had geared wheels. Gears also have ancient roots in other parts of the world, with Aristotle documenting the use of a rotating wheel that turned another wheel in the opposite direction in the fourth century B.C.E. 


Essentially, gears are rotating mechanical parts with teeth cut into the exterior that allow them to connect with other pieces and transmit rotational motion. By effectively using gears, they can change the speeds and direction of power that a machine uses. 


Spur gears are the most common type of gears, efficiently transmitting power into motion from one parallel shaft to another. Based on the number of teeth of the driving gear, the drive speed can be reduced or increased. 


Gears are a key part to our modern machines. Many complex pieces of equipment rely on precision gears, perfectly designed to meet specific needs. SDP/SI manufacturers custom gears and complex gear assemblies for many of the most well-known companies in the aerospace, medical and robotics industries. By engineering and manufacturing your gears in house, we can meet your requests faster and more precisely. 

 

Understanding Different Gear Types

While spur gears are the most common, they are not the only option. There is a large variety of gears that vary based on application, manufacturing requirements, shape, size and more. Our precision and commercial, standard and custom gear manufacturing capabilities include:

Spur Gears

Spur Gears have teeth parallel to their axis and a cylindrical shape. It is also the easiest of the gears to manufacture and has the greatest number of applications.

Helical Gears

Helical Gears are cylindrically shaped gear with helicoid teeth. An advantage of helical gears are they can bear more load than spur gears and they run quieter. A disadvantage is the axial thrust force the helix form causes. Helical gears are widely used in industry.


Helical gears have a higher tooth strength due to the elongated helical wraparound tooth base support. There is also greater tooth overlap, creating a larger contact ratio, this is what allows them to carry more weight. 


Parallel helical gears, which transfer power between parallel shafts, and crossed helical gears, which transfer power between non-parallel shafts, are the two main types of helical gears.

Double Helical Gears

This is a gear with both left-hand and right-hand helical teeth. The double helical form balances the inherent thrust forces.

Screw Gears (Crossed Helical Gear)

Two helical gears of opposite helix angles will mesh if their axes are crossed. As separate gear components, they are merely conventional helical gears. Installation on crossed axes converts them to screw gears. They offer a simple means of gearing skew axes at any angle. Because they have point contact, their load carrying capacity is very limited.

Internal Gears

Internal gears are cylindrical shaped gears with their teeth inside the circular ring. They can mesh with a spur gear and are often used in planetary gear systems.

The way internal gears mesh is dependent on specific dimensions including gear size (pitch diameter) and the angle of the teeth on the gear;  proper calculations are required to ensure an accurate fit. 

When utilizing internal gears, there is potential for excessive noise, premature tooth wear, and vibration in the gear train. The three different types of interference causing these issues include: 

  • Involute Interference – often due to the use of a pinion with too few teeth where one gear tooth's non-involute portion comes into contact with the other gear tooth's involute portion.
  • Trochoid Interference - occurs when there are more contact points due to the tooth profile's deviation from the ideal involute curve.
  • Trimming Interference - When trying to pull the meshing gears apart, radial interference occurs, making it impossible to separate them properly.

Properly cut and applied internal gears excel in systems needing high reduction ratios (slowing things down in a single step). They work great in compact situations such as for robotics or heavy machinery. 

Spur Racks

This is a linear shaped gear which can mesh with a spur gear with any number of teeth. The spur rack is a portion of a spur gear with an infinite radius.

 

 

Helical Racks

This is a linear shaped gear which meshes with a helical gear. Again, it can be regarded as a portion of a helical gear with infinite radius.

Viewed in the normal direction, the meshing of a helical rack and gear is the same as a spur gear and rack. However, you can also perform calculations related to helical racks in the radial system (such as when it’s perpendicular to a gear’s axis). 

Face Gears

This is a pseudo-bevel gear that is limited to 90° intersecting axes. The face gear is a circular disc with a ring of teeth cut in its side face, hence the name face gear. Tooth elements are tapered towards its center. The mate is an ordinary spur gear. It offers no advantages over the standard bevel gear, except that it can be fabricated on an ordinary shaper gear generating machine.

Straight Bevel Gears

This is a gear in which the teeth have tapered conical elements that have the same direction as the pitch cone base line (generatrix). The straight bevel gear is both the simplest to produce and the most widely applied in the bevel gear family.

Spiral Bevel Gears

This is a bevel gear with a helical angle of spiral teeth. It is much more complex to manufacture but offers a higher strength and lower noise than other bevel gear pairs.

Worm And Worm Gears

Worm set is the name for a meshed worm and worm gear. The worm resembles a screw thread; and the mating worm gear a helical gear, except that it is made to envelope the worm as seen along the worm’s axis. The outstanding feature is that the worm offers a very large gear ratio in a single mesh. However, transmission efficiency is very poor due to a great amount of sliding as the worm tooth engages with its mating worm gear tooth and forces rotation by pushing and sliding. With proper choices of materials and lubrication, wear can be contained, and noise is reduced.

Double Enveloping Worm Gears

This worm set uses a special worm shape in that it partially envelops the worm gear as viewed in the direction of the worm’s gear axis. Its big advantage over the standard worm is a much higher load capacity. However, the worm gear is very complicated to design and produce.

Zerol Gears

Zerol gears are a special case of spiral bevel gear. It is a spiral bevel with zero degrees of spiral angle tooth advance. It has the characteristics of both the straight and spiral bevel gears. The forces acting upon the tooth are the same as for a straight bevel gear.

Hypoid Gears

This is a deviation from a bevel gear that originated as a special development for the automobile industry. Hypoid gears permit the drive to the rear axle to be nonintersecting and thus allow the auto body to be lowered. It looks very much like the spiral bevel gear. However, it is complicated to design and is the most difficult to produce on a bevel gear generator.

 

Key Benefits of Gear Usage 

Many mechanical devices heavily rely on the ability to transmit power and motion between rotating shafts. Gears make this possible while still maintaining uniform motion and reliability. 

Gears are heavily relied on for their ability to:

  • Offer positive transmission of power.
  • Range in size from small miniature instrument installations, that measure in only several millimeters in diameter, to huge powerful gears in turbine drives that are several meters in diameter.
  • Provide position transmission with very high angular or linear accuracy, such as used in servomechanisms and military equipment.
  • Couple power and motion between shafts whose axes are parallel, intersecting, or skewed.
  • Can be easily interchanged due to standardizations in accordance with size and shape.

What is the Law of Gearing?

Gears must have consistent angular velocities or proportionality of position transmission. Accurate placement is required for precision devices. In order to work correctly, high-speed and/or high-power gear trains must also be transmitted at constant angular velocities to avoid issues such as vibrations, excessive wear, or noise.

Conjugate gears are gears with a tooth profile that mesh and allow for constant angular velocity. This “conjugate action” means that your gears’ relative velocities stay consistent while in motion. 

Shown in the image above, your gears will meet at the “pitch point” along the line of centers. Establishing this point can help you begin to calculate exactly what the velocity ratio is for two specific gears. 

In the figure above, the tangent to the two base circles represents the line of contact, or line-of-action in gear vernacular. The pitch point, P, is defined as the point at which this line crosses the line of centers. This sets the size of the pitch circles, also known as pitch diameters.

The Law of Gearing states:

"A common normal to the tooth profiles at their point of contact must, in all positions of the contacting teeth, pass through a fixed point on the line-of-centers called the pitch point." Any two curves or profiles engaging each other and satisfying the law of gearing are conjugate curves." 

Common Gear Applications and Uses

Gear Manufacturing for Aviation and Defense Industries

Precision is paramount for customers working in aviation and defense. There is often no room for error. Custom manufactured gears and gear assemblies make innovation possible while still adhering to strict quality standards. 

Applications include a wide range of military and commercial aircraft, robots, satellites, UAVs, tanks, missiles, and even the Mars Rover.

  • Actuation/positioning systems
  • Antenna positioning
  • Cargo movers
  • Door releases
  • Ejection systems
  • Flight guidance controls
  • Fuel control
  • Gimbals
  • Gun turrets
  • Instrumentation
  • Pan and tilt cameras for surveillance and security
  • Positioning systems
  • Rudder control
  • Solar wing positioning
  • Stabilization systems
  • Structural components
  • Weapons targeting

Precision Custom Gears for Industrial Manufacturing

Successful industrial manufacturing is the backbone to modern society. Gears, assemblies, and gear boxes are key components to manufacturing equipment.

Our engineers and manufacturing teams routinely partner with OEMs, providing the individualized customer support each project merits. With proven performance and unsurpassed experience, our engineers are here to help during the concept and early design stages of a project.

 

Custom Gear Solutions for Medical Technology 

As medical technology has evolved, gears have remained a staple component for many tools. Our expertise spans various medical applications, including nebulizers, insulin pumps, dialysis equipment, minimally invasive surgical devices, and intricate surgical robots.

Medical technology relies on tailored solutions and manufacturable concepts. From fabricating individual components to designing complex prototypes, our team is your trusted partner. Applications across medical tech include everything from robotics to drug delivery devices.

  • Minimally invasive and surgical gear drivers
  • Pharmaceutical processing & packaging
  • Therapeutic and assisted living devices
  • Printing and recording devices
  • Patient positioning
  • Surgical robotics
  • Robotic surgical arms
  • Miniature components for drug delivery devices

Automation and Robotics Custom Gear Manufacturer

Gear manufacturing plays a fundamental role in the development and functionality of robotics, as gears are critical components that ensure precision, motion control, and power transmission within robotic systems. 

Our cutting-edge manufacturing facility and highly qualified staff guarantee that we are consistently selected to work on projects that push the boundaries of contemporary gear manufacturing by creating solutions for a changing world, advancing automation by succeeding where other manufacturers have failed. 

Robot designers and OEMs benefit from engineered solutions that help make their robots smaller, faster and lighter. Applications include medical uses and manufacturing purposes.

  • Robotic-assisted surgery devices
  • Warehouse automation
  • Automated guided vehicles 
  • Autonomous mobile robots

Standard and Custom Gears Primed for Your Projects

The manufacturing of standard and custom gears requires a high level of precision. When engineered and used correctly, gear types such as spur gears, bevel gears and worm gears can be employed across a vast range of applications. 

By utilizing comprehensive engineering experience and a meticulous manufacturing process, SDP/SI applies strict quality control for all standard and custom gears, racks and gear assemblies. 

Our gear capabilities range from various metal and plastic materials and are available in inch and metric sizes. Shop our full range of precision gears, racks, and pinions or contact us for custom solutions. 

We can't find products matching the selection...

Questions? Contact Our Team

Give us a call at 516-328-3300 or fill out the form below and our team will be in touch soon. *marks required fields.


Custom Solutions

Looking for a custom solution? Contact our engineers.

contact our team